6/16/2011 10:11 PM | |
Joined: 4/20/2007 Last visit: 2/6/2024 Posts: 724 Rating: (41) |
seems I learned something today to... Just curious here.. So when he comes over the 8000 something value, the place for storing the value is getting to large? What if he makes sure the value got less decimals? That would solve a bit of the problem? |
6/17/2011 7:24 AM | |
Joined: 10/7/2005 Last visit: 4/28/2024 Posts: 3004 Rating: (1046)
|
Have a look at the FAQ below guys, it will (should) answer all your questions: How accurately can I calculate with REAL numbers that are used in extensive formulas? |
Cheers |
|
This contribution was helpful to1 thankful Users |
6/17/2011 7:33 PM | |
Joined: 4/20/2007 Last visit: 2/6/2024 Posts: 724 Rating: (41) |
I just meant the value he mentioned 8192 |
6/17/2011 8:27 PM | |
Posts: 8946 Rating: (999) |
Here is a very easy example to show the problems with real - resolution.
AttachmentGleitpun.zip (74 Downloads) |
Follow us on