6/22/2011 4:31 PM | |
Joined: 4/24/2006 Last visit: 5/3/2024 Posts: 8632 Rating: (1148) |
Hello, I guess you mean this link: Why does a message appear in STEP 7 stating that there is not a license key present even though the relevant license key is installed? Can you open Automation License Manager and check status of License Key Step 7? Best regards, Wizard |
3/20/2020 11:37 AM | |
Joined: 4/28/2017 Last visit: 3/14/2024 Posts: 149 Rating: (24) |
HelloANUJ9891i , Which version of ALM are you using? And, was that ALM installed along with this Step 7 installation or by different setup? Also, Can you please attach the image of your ALM status by showing the License info. You can even hide your License no. Which user account is active right now? It will be better if you share the User group list as well. |
Note: If this post did really help you, you may use the "Rate" button to express your support, Thank you. |
|
3/21/2020 6:35 PM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (836)
|
Hello, It's very important to know if SW is Step7 V5.6 or V5.6 + SP1. Also Version of ALM is very important. Please check the comptability between them as well as with OS using the attached file. Hope this helps. AttachmentSTEP-7_V5.6_compatibility-list_en_2020-03-02.xlsx (938 Downloads) |
Ayman Elotaify |
|
This contribution was helpful to1 thankful Users |
Follow us on