7/28/2011 2:48 PM | |
Posts: 739 Rating: (55)
|
Hello, it is possible, that the power surge destroyed the voltage measurement in the DC-Link of this two inverters |
9/7/2011 1:15 PM | |
Joined: 8/18/2009 Last visit: 6/17/2024 Posts: 548 Rating: (33) |
Hi then what necessity activity to solve the problem. |
Rajkiran Patil |
|
9/9/2011 3:13 PM | |
Posts: 739 Rating: (55)
|
P0210 is not needed to change! Parameter P0210 defines the supply voltage. Its default value depends upon the type of inverter. e.g.: P0210 = 230V the mains operating voltage = 1 AC 200 V to 240 V or 3 AC 200 V to 240 V P0210 = 400V the mains operating voltage = 3 AC 380 V to 480 V It is not possible to change from 230 to 400V or from 400 to 230V! I suggest cheking technical details of inverter and application, and starting setup again following the Getting Started. http://support.automation.siemens.com/WW/view/en/38645759 |
Follow us on