8/2/2011 11:39 PM | |
Posts: 133 Rating: (2) |
with 314c-2dp (bought in 2005), and CP343-1 (to buy) it is possible to use Knx/eib2s7; i don t understand if it works with all S7-300 CPU thank you
|
8/3/2011 12:06 PM | |
Joined: 8/25/2005 Last visit: 5/2/2024 Posts: 1161 Rating: (110) |
Hello automation_1, have a look here: KNX/EIB2S7 Editor and Function Blocks for Commuication to KNX/EIB BUS over ETHERNET : version 1.0 Did you find your hardware there? Think with the correct CP it should work. But never tested it. Best regards Sabine |
8/3/2011 4:22 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (306) |
Hello, In this entry you will see which HW is supported by V1.0 http://support.automation.siemens.com/WW/view/en/46374645 The CPU 313 is not listed. |
Best regards |
|
11/26/2012 9:25 PM | |
Posts: 133 Rating: (2) |
Thanks |
4/3/2018 8:41 AM | |
Joined: 6/19/2017 Last visit: 5/7/2024 Posts: 8001 Rating: (163) |
New question published by CanMurat_KNX is split to a separate thread with the subject SIMATIC S7-400H CPU-416-5H Want to use KNX/EIB2S7 to communicate with KNX bidirectional. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on