12/5/2011 9:14 AM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating: (1166)
|
Dear Arun Steer, You should try to perform an OS update, with the option Reset to Factory settings. Have a look at this link: What settings do you have to make on an MP 377 to reset the operator panel to the factory settings? Best regards, Wizard |
12/5/2011 9:39 AM | |
Joined: 4/29/2010 Last visit: 7/15/2024 Posts: 1557 Rating: (161)
|
Hello, can you operate something on the screen via the touch or can you operate nothing in this case? best regards |
1/13/2016 1:21 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating: (123) |
New question published by eki856 is split to a separate thread with the subject MP377 15 " Touch screen not working. Best regards |
Follow us on