12/6/2011 5:39 PM | |
Joined: 10/26/2011 Last visit: 10/1/2024 Posts: 762 Rating: (191) |
Hello Plankman, I heart about a similar effect. The reason was, that the setting of the arrangement of the monitors was wrong. The Windows setting was not the same as the setting in WinCC. Windows and WinCC arrangement of the monitors have to be the same: 1 2 3 4 => WinCC help under Multi-VGA If the settings are different, the "GetScreen"-function makes strange things. Parts of faceplates are not visible or on the false monitor Regards Thunderstorm |
SIMATIC PCS 7 - Overview |
|
This contribution was helpful to1 thankful Users |
Follow us on