1/3/2012 9:59 AM | |
Posts: 2 Rating: (0) |
in which parameter of driver cani read the driver output current and current's mA value? |
1/3/2012 11:27 AM | |
Joined: 6/4/2008 Last visit: 6/27/2024 Posts: 1485 Rating: (323)
|
Hi mfk, unfortunately, you cannot!! Instead, you have to read a value which is a scaled representation of the variable plugged into the Analog output. I have "assumed" you are referring to CUVC. For example, if you placed "Speed Actual" (KK148)into the analog output (P640.1), then this would be scaled in percentage according to the reference parameter for speed (P353) See the function diagrams 81 and 83 in the compendium available here. http://support.automation.siemens.com/WW/view/en/13472409 Regards, Graeme |
Follow us on