1/23/2019 2:06 AM | |
Joined: 10/17/2007 Last visit: 4/22/2024 Posts: 3972 Rating: (340)
|
From you picture I know you have old SIMODRIVE 611 drive system--it is one generation before 611A, Actually I have been worked in the Siemens Factory which made this drive in Germany as finial inspection technician. I have had the paper book which you need, but I cannot find it now. I attached the old 611A manual 1997 Edition , check ch. "VS" , there are forms you need. They not 100% matching your drive, but similar. 611 use 400DC bus the 1FT5.. motor suite this 611A use 600DC bus the "newer" 1FT5... motor suite that. so in the manual/ form I attached --you will find the motor number may not match your motor so you can only use the book as reference By the way --even I answer your question, But I don't know why you need that form, if you change drive module (box) nothing to do with that small sub-module, taking it out remember S2 setting and don't change any switch. may be you only want to know how to set up S2. then read the book I attached will help you Do you know--if you old 611 defective, you have option to replace by newer (still old ) 611A control card and drive box with the same ampes --such as 12/24 A (611) replaced by 25 A (611A) ** after I finish the answer --I found you post anther one question, which was also answered by me--That is not so good, you need focus on one topic--But I know now why you need that form--so I think the book i attached will help you --as you 2nd motor may including in the form If you think my answer help you a little , can you please rate my post --in the bottom
Attachment611A_IA.PDF (260 Downloads) |
Last edited by: nulizhang at: 1/23/2019 2:07:50 AMIf you think my answer help you a little , can you please rate my post Last edited by: nulizhang at: 1/23/2019 2:09:16 AMLast edited by: nulizhang at: 1/23/2019 2:15:41 AMIf you like my comments please |
|
This contribution was helpful to1 thankful Users |
Follow us on