Industry Online Support
Technical Forum
5/7/2007 8:15 AM | |
Joined: 10/11/2006 Last visit: 9/18/2024 Posts: 5906 Rating: (804)
|
Hello, X9/4,5 is not used in case of compact type and it is the control output for the main contactor in case of chassis type (it can be "missused" for the brake, if there is no main contactor, by connecting P601 to the braking control). The brake can be controlled using the function "braking control"from function diagram 470. Attached the diagrams for X9 and brake control. Best regards TechTeam Attachmentvc34_kompend_fp01_e.pdf (520 Downloads) |
With best regards, |
|
Follow us on