3/20/2012 1:09 PM | |
Joined: 2/21/2011 Last visit: 4/18/2024 Posts: 52 Rating: (12) |
Hello miskopeter, I think this link will help you: SINAMICS S120 Firmware Version 4.4 HF12 http://support.automation.siemens.com/BR/view/en/48736528 Best Regards, Henrique Barlera |
3/21/2012 4:24 PM | |||||
Posts: 8 Rating: (0) |
Hello thank you but i can not see this document because:
|
||||
1/6/2015 12:36 PM | |
Posts: 8 Rating: (0) |
I have the same problem with CU320 (F30611) 6SL3040-0MA00-0AA1 how to resolve it?
|
1/7/2015 1:15 PM | |
Joined: 10/11/2006 Last visit: 9/26/2024 Posts: 5907 Rating: (804)
|
Hello, what is the fault code? F30611 (x)? If the old CU 6SL3040-0MA00-0AA1 is used then F30611 (1951) cannot occur as the fault code 1951 is implemented in the FW4.4 and above. Thefastest way to solve your issue is to open a Service Request: http://www.siemens.com/automation/support-request |
With best regards, |
|
1/7/2015 4:35 PM | |
Posts: 8 Rating: (0) |
Thanks for your answer, i sent a request but as you said they need the code, and i don't know where to find this code |
1/7/2015 5:22 PM | |
Posts: 8 Rating: (0) |
all that i see in the screen is 05 F30611 and i have also these faults F30600 and F01600
|
Follow us on