2/24/2014 5:10 PM | |
Posts: 340 Rating: (6) |
new question is splittet to If 20mA is 27684, what's 4mA should be in NORM, 0 or 5336? 6ES7 231-4HD32-0XB0. |
3/26/2018 10:22 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by tvr126 is split to a separate thread with the subject connect a loop powered transmitter that outputs 4-20 mA. Best regards |
Follow us on