5/15/2012 11:24 PM | |
Joined: 5/27/2009 Last visit: 8/14/2024 Posts: 122 Rating: (8) |
Hi everyone, some days ago i was making test with Windows 2008 Ent R2 64 bits Server and WinCC v7SP3, i tested a Client-Server connection and it worked...but unfortunately we have compatibility issues with another software and we had to change Windows to Windows 2008 SP2 32bits, Server was configured again with same options but now Clients can't connect. If i tried to launch the project trough the shared folder WinCCExplorer Opens and ask for user and password but as soon as i entered it shows "Server not Available". I dont know why now its not working. I have the same subred and network segment, same workgroup, SIMATIC HMI Permissions, Licenses Ok. I have tried to open with simatic shell also but i get an error when i tried to interconnect i only can activate or deactivate remote. Hope someone can help. Thank u. AttachmentError.zip (675 Downloads) |
5/16/2012 2:15 PM | |
Joined: 10/20/2009 Last visit: 4/3/2017 Posts: 215 Rating: (12) |
Hi zein, Have you checked compatibility of your new Windows OS with PCS7 software. You can check that on link below: https://support.automation.siemens.com/kompatool/pages/main/index2.jsf Check these things in your Server & Clients - 1. Check your workgroup name. It should be same in all PC's. 2. Check the User Name & Password. It should be also same for all PC's. And all admin rights to be given to this user name. 3. Network Card Drivers should be installed on all PC's. 4. Check the permission of Shared Folder. It should have complete access. 5. Also, Check whether OS Assignment is done for the Clients. 6. Check your PCS7 installation on all PC's |
Last edited by: R J at: 5/16/2012 2:17 PMRegards, |
|
Follow us on