2/11/2013 2:32 PM | |
Joined: 7/7/2010 Last visit: 7/16/2024 Posts: 14954 Rating: (2393) |
Maybe the object type VIEW_IN means something to you in your TP600 project? I have had several similar errors that to me were less than helpful. My fix has been to create a new screen, go to the old screen, ctrl-a to select all, ctrl-c to copy all, go to new screen, ctrl-v paste, and then make buttons and plc logic that push the screen to go to the new screen. Then lastly, delete the screen causing problems. Compile and magically it works (most of the time). Once while waiting on Siemens to help correct a compile problem, I simply created a brand new HMI in my existing project, then copied every piece from the original HMI to the new HMI. It took a couple of hours to get it done, but it did compile and work afterwords. The strange part is the response from local Siemens support was they could readily duplicate the problem. After sending to corporate HQ support, suddenly they could not get the problem to appear. Was I shocked? No. I suspected it was a default language issue as I have English as the default language, and of course corporate HQ has Deutsch (German). I have tested broken HMI projects in the past by changing the default language to German, compiles fine, then change back to english and continues to compile fine afterwards. Please submit your project to Siemens via their Support Requestsystem so they can verify it is fixed in V12. They may also find what workaround is possible. |
science guy |
|
1/15/2016 12:20 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating: (123) |
New question published by Yves_Bosmans is split to a separate thread with the subject TIA Portal V13, internal ERROR. Best regards |
Follow us on