(24)| 7/29/2013 2:47 PM | |
|
Posts: 5 Rating:
|
To install STEP 7 v5.5 SP3 (DVD update release) follow these steps. 1. Download and install the latest 64-bit version of automation licence manager. http://support.automation.siemens.com/WW/view/en/114358 2. Copy DVD content to any directory on hdd. 3. Modify ./Setup.exe using any resouce modification software. Eg ResourceHack. Add the line <supportedOS Id="{4a2f28e3-53b9-4441-ba9c-d69d4a4a6e38}"></supportedOS> //this is the os ID of Windows 8 64bit 4. Modify ./InstData/Setup.ini under section OS. PlattformIDAllowed = 1;2;3 Add the lines Win8x64=1 5. Modify all msi-files to enable the ingore-button on installation failures (like installing on unsupported OS's). Use any software possible to manipulate MSI-files. E.g. InstEd. Search for DLG_INSTALLATIONREQUIREMENTS_DISABLE_IGNORE. Change Action from Disbale to Enable. Run ./Setup to start installation. Press the ingore-button when told it's not possible to install on running OS.Good luck! Disclaimer. I can not be held responsible to any result caused by following this guide. It's just for educational purposes. |
This contribution was helpful to
|
|
| 9/6/2013 11:48 AM | |
|
Joined: 9/11/2011 Last visit: 9/10/2024 Posts: 53 Rating:
|
Thanks friend |
| 1/5/2014 11:56 AM | |
|
Posts: 21 Rating:
|
Dear sir I need more explanation. because i can't follow your method and i still can't install it thanking you |
| 3/21/2014 12:42 PM | |
|
Posts: 1 Rating:
|
hello i'm be so happy if you learn us with picture to how do this rule you said in this post. tnx |
Follow us on