9/25/2013 1:25 AM | |
Posts: 76 Rating:
|
I have also estimated similar problem. I have not the original project online by ethernet and profibus not lose the whole project achievement. sinamics_integrated1 message me offline and download the program does not download "i / o device variables" download only a part of D425 I have installed v4.3 scout will I need a 5611 for example? and I communicate by the Profibus interface of the plc s7 and reaches a maximum speed of 1.5 Mbps diagnosis device attached
AttachmentDevice Diagnostics.zip (641 Downloads) |
4/19/2018 9:08 AM | |
Joined: 6/19/2017 Last visit: 6/28/2024 Posts: 8176 Rating:
|
New question published by AutoGen_543688 is split to a separate thread with the subject uploading simotion D455. Best regards |
Last edited by: Jen_Moderator at: 4/19/2018 9:11:40 AMInserted right headline. My Forum is the place to personalize your profile, |
|
Follow us on