10/4/2013 9:25 AM | |
Joined: 8/22/2011 Last visit: 5/23/2024 Posts: 52 Rating: (0) |
Dear experts, can i use this password BBHÿ@bb for logo ? and how i can use the unicode in password? Best Regards |
10/4/2013 10:11 AM | |
Joined: 11/23/2011 Last visit: 5/14/2024 Posts: 202 Rating: (32)
|
Hello bassel_almouie, which version of LOGO! module do you have? I would recommend as in the manual described to use uppercase letters with a maximum lenght of ten characters. You can also have a look to the section "Assigning a program password from the LOGO! Basic" on page 92 of the actual manual: http://support.automation.siemens.com/WW/view/en/50074616 Hope this helps you. Greetings, KM_AS |
10/4/2013 10:24 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hi bassel_almouie, Refer to manual: A password can have a maximum length of 10 characters, and consists only of uppercase letters. |
Last edited by: Ste39 at: 10/4/2013 10:25 AM |
|
Follow us on