11/28/2014 10:45 AM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928) |
Harry, It is not the intion to modify thestandard Siemens blocks!Like OP already did, you can change the text in the identifier column. Do you have your language setup properly? Simatic Manager takes over the regional language settings, but WinCC uses unicode. If you use a language not supported by PCS7 problems can occur. Also check if you use the correct language in WinCClike mark said. |
If I could help you, you can use the RATE button. Thank you. |
|
12/1/2014 6:17 AM | |
Joined: 2/21/2014 Last visit: 3/14/2024 Posts: 652 Rating: (342) |
Hi Orecaand All, Sorry for that reply. I am aware that Block code should not be modified, and mostly it will not be available also for modification. I am working on SCL code for some blocks and I am modifying the code everyday, thereforit slipped my mind. in the flow of my work, I replied to modify the SCL code. |
Last edited by: HarrY ji at: 12/1/2014 6:18 AMI Need to be careful now onwards before replying. You can always use "Rate" and "To Thank" button to appreciate my efforts in helping you :) |
|
12/18/2014 9:51 AM | |
Posts: 44 Rating: (2) |
Thanks for the help all. For some reason after half a dozen recompiles it suddenly 'took'. No idea why, but your suggestions were great for troubleshooting |
Follow us on