2/2/2016 3:55 PM | |
Posts: 15 Rating: (0) |
I hope I am not intruding here. I cannot back up from TP 700 comfort with prosave (v13). Even if I connect with MPI or ethernet. At first it shows that the connection has been established but after a few seconds it shows the message that the back up is canceled. The weird thing though is that the HMI screen saws the progress bar going up until it completes the back up. But there is no back up. I've checked the connections and everything but to no avail. The screen is new, with the program from the provider. Could it be locked or something? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 2/3/2016 10:58:19 AMNew subject after splitting |
|
9/19/2016 9:01 PM | |
Joined: 1/21/2016 Last visit: 4/22/2023 Posts: 83 Rating: (1) |
i think you should use mini b/usb cable mpi pn is for download too but try mini-b/usb Attachmenthmi connection cables.xls.zip (394 Downloads) |
Last edited by: amrelhajali at: 9/19/2016 9:02:53 PMLast edited by: amrelhajali at: 9/19/2016 9:08:29 PMAmr Ali |
|
10/26/2016 10:23 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by arabi1982 is split to a separate thread with the subject How I can reset or Delete the password?. Best regards |
Follow us on