Bit access in array of Dint with variable index
Bit access in array of Dint with variable index (5)
 (5)| 12/9/2014 5:18 PM | |
| Posts: 5225 Rating: 
 | -- | 
| Last edited by: William B. at: 12/9/2014 5:33 PM[delete message] | |
| 12/9/2014 9:32 PM | |
| Posts: 5225 Rating: 
 | ..design idea attached when using AT overlay - when available. Note that the DINT is now DWORD. For handling DINT a convert network is required. w | 
| 12/16/2014 5:04 PM | |
| Posts: 5225 Rating: 
 | I hear you and having worked on some other environments, I can agree with you. But hey... we work with what we have; if you can adapt - then you'll be doing fine. The main thing is to get the job done. Note that in the Siemens family there are various options - depending on what processor you use under which software. Greetings. w Late Note: You may wish to page to the following tip: [LINK] There are detail notes in following posts that might be of value. | 
| Last edited by: William B. at: 12/16/2014 5:11 PMadd late note | |
| 12/28/2017 12:51 PM | |
| Joined: 9/6/2011 Last visit: 9/23/2025 Posts: 22 Rating: 
 | Maybe this would be useful for someone. The main idea is to use AT overlay access. | 
Follow us on