3/29/2021 8:35 AM | |
Joined: 7/19/2010 Last visit: 8/14/2024 Posts: 34 Rating: (3) |
This is my simple circuit. It doesn't work. How can I trigger the timer? |
3/29/2021 8:36 AM | |
Joined: 12/18/2014 Last visit: 9/23/2024 Posts: 33823 Rating: (4203)
|
Who switches V1.2? |
3/29/2021 8:53 AM | |
Joined: 7/19/2010 Last visit: 8/14/2024 Posts: 34 Rating: (3) |
I set it through a desktop application I have developed and it works fine without the timer. |
3/29/2021 8:55 AM | |
Joined: 12/18/2014 Last visit: 9/23/2024 Posts: 33823 Rating: (4203)
|
V1.2 comes as a static signal? |
3/29/2021 9:10 AM | |
Joined: 12/18/2014 Last visit: 9/23/2024 Posts: 33823 Rating: (4203)
|
You don't know if the signal is static or dynamic? If the signal is a static signal, the timer are always high. |
Follow us on