4/7/2021 7:18 PM | |
Joined: 11/28/2020 Last visit: 4/23/2024 Posts: 5 Rating: (0) |
hey thx for helping me with the analog output dim with pushbutton i have a next question i want to dim with a puschbutton and i want to dim the same analog output with LWE software pushbutton on my mobile device i buy new logo 8.3 and in the LWE there is a pusch button but when i pusch the button so long that i push there change nothing there is only a signal when i release the button works like a high edge signal and a low edge signal ------------------------------------------------------------------------------------------ |
Last edited by: orelio at: 04/07/2021 19:59:47Last edited by: Jen_Moderator at: 04/08/2021 09:26:28New subject after splitting |
|
4/7/2021 8:00 PM | |
Joined: 11/28/2020 Last visit: 4/23/2024 Posts: 5 Rating: (0) |
ok next time a make a nother post sorry |
This contribution was helpful to1 thankful Users |
4/8/2021 4:21 AM | |
Joined: 12/18/2014 Last visit: 5/7/2024 Posts: 32988 Rating: (4076)
|
Try this ... I must set the time higher, now it is 1.0s. 0.5s is too short by push button via ethernet. And next time please write which LOGO! you have ... Attachmentorelio.zip (170 Downloads) |
Follow us on