4/8/2021 4:30 PM | |
Joined: 12/7/2016 Last visit: 12/25/2023 Posts: 29 Rating: (0) |
Is there any migration manual from MP 370 to TP, Comfort series? I found just manual for MP377 series There it is TP1900 recomended for MP377 replacing As I have read here, we can use also TP1500 Instead (but why tp1900 is recommended?) What means "you can only compare the old with the new HMI devices using the display size to a limited extent"? In my opinion it means that project must be changed manually, migration is not complete solution. Some troubles can appear after migration. You can see them under links to different topics. So it is better to have full sequential algorithm of a) panel selection b) migration process description with actual list of software versions that are needed. c) actions to eliminate all troubles after migration WinCC Flexible 2008 Migration : ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/09/2021 08:27:15New subject after splitting Last edited by: Fedia at: 04/16/2021 16:03:19Last edited by: Fedia at: 04/16/2021 16:13:59Last edited by: Fedia at: 04/16/2021 16:14:45 |
|
4/16/2021 9:49 AM | |
Joined: 12/7/2016 Last visit: 12/25/2023 Posts: 29 Rating: (0) |
mp-370-to-mp-377-migration-trouble |
Last edited by: Fedia at: 04/16/2021 15:15:05Last edited by: Fedia at: 04/16/2021 15:16:59Last edited by: Fedia at: 04/16/2021 15:20:49Last edited by: Fedia at: 04/16/2021 15:22:18Last edited by: Fedia at: 04/16/2021 15:24:44 |
|
5/12/2021 11:26 AM | |
Joined: 12/7/2016 Last visit: 12/25/2023 Posts: 29 Rating: (0) |
|
5/19/2021 4:32 PM | |
Joined: 12/7/2016 Last visit: 12/25/2023 Posts: 29 Rating: (0) |
|
Last edited by: Jen_Moderator at: 05/20/2021 08:19:24Optimized link. |
|
7/13/2021 1:36 PM | |
Joined: 12/7/2016 Last visit: 12/25/2023 Posts: 29 Rating: (0) |
And what means those? 1. "the source project contains one or more disabled animations" 2. "Exception in client upgrade hook: The project or library possible contains data that cannot be upgraded by the currently installed software" Very good question: PEData.plf could not be upgraded 2 PEData.plf' could not be upgraded. |
Last edited by: Fedia at: 07/13/2021 13:36:44Last edited by: Fedia at: 07/13/2021 13:36:58Last edited by: Fedia at: 07/13/2021 13:45:04Last edited by: Fedia at: 07/13/2021 13:45:35Last edited by: Fedia at: 07/13/2021 13:47:07Last edited by: Fedia at: 07/13/2021 13:47:35Last edited by: Fedia at: 07/13/2021 14:16:39Last edited by: Fedia at: 07/14/2021 08:50:43 |
|
Follow us on