4/20/2021 12:45 PM | |
Joined: 9/9/2015 Last visit: 10/19/2022 Posts: 22 Rating: (0) |
Hello! Windows 10 Simatic Manager v5.6 When working in HW Config I can't erase the device Best regards. |
4/20/2021 12:47 PM | |
Joined: 5/12/2006 Last visit: 9/20/2024 Posts: 22365 Rating: (3011) |
any message? maybe the project is write protected, this should be informed in a message if you open the project. |
4/20/2021 12:52 PM | |
Joined: 9/9/2015 Last visit: 10/19/2022 Posts: 22 Rating: (0) |
a normal project, I can make changes in the program |
4/20/2021 1:01 PM | |
Joined: 5/12/2006 Last visit: 9/20/2024 Posts: 22365 Rating: (3011) |
can you provide some screens? Which devices you try to delete/erase? |
4/20/2021 1:10 PM | |
Joined: 9/9/2015 Last visit: 10/19/2022 Posts: 22 Rating: (0) |
|
4/20/2021 2:21 PM | |
Joined: 9/21/2012 Last visit: 9/20/2024 Posts: 4148 Rating: (464) |
What if you just try to select and delete one device at a time? |
4/21/2021 6:37 AM | |
Joined: 9/9/2015 Last visit: 10/19/2022 Posts: 22 Rating: (0) |
I do so, it can be seen even in the screenshot, only one device is selected. |
Follow us on