4/30/2021 12:40 AM | |
Joined: 5/11/2016 Last visit: 9/5/2022 Posts: 18 Rating: (0) |
Erro de entrada: a versão do módulo ou o uso simultâneo do módulo TIA PORTAL V13 SP1 Up9 Preciso de ajuda. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/30/2021 09:37:53New subject after splitting Blanco Automação |
|
4/30/2021 3:50 AM | |
Joined: 12/18/2014 Last visit: 9/20/2024 Posts: 33801 Rating: (4199) |
Hello BlancoAutomacao, this is a english speaking forum. Please be so kind and write your next posts in english.
And please don't post twice for the same problem. You post also in this topic (6th reply): ET200 parameter assignment errorAnd you made also a own topic: ET200 IM155-6PN ST |
Last edited by: ixo65 at: 04/30/2021 03:55:48 |
|
This contribution was helpful to1 thankful Users |
4/30/2021 9:40 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice. The second thread with the subject Input error: the module version or the simultaneous use of the module is published within the conference Decentral Peripherie. Jen_Moderator |
Follow us on