5/2/2021 1:48 PM | |
Joined: 9/27/2006 Last visit: 4/26/2024 Posts: 12257 Rating: (2665) |
Hello SalarAkbari; Besides the many simalr threads and documents on the forum site, there are web searches that can result in interesting finds, suc as this one: https://www.programmersought.com/article/872156467/ Basically: prepare the gsd file for the S7-1200 configuration as a Profibus slave (in TIA Portal), setup the data exchange areas for the input and output areas (including the required data for your drive). Then import the gsd file for the CM 1242-5 in your master (with its own Profibus configuration software), setup data exchange similar to the ones setup in the CM 1242-5 except for one important detal: all data exchange marked as "I" in the S7-1200 become "Q" in the master (same size, same type); conversely all data exchanges areas marked as "Q/" in the slave must become "I" in the master configuration. I think that if you follow the well-explained steps in thos document you shold be able to estavlish your Prodibus link without too many problems. Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
Follow us on