5/3/2021 1:02 PM | |
Joined: 4/16/2021 Last visit: 6/6/2022 Posts: 26 Rating: (0) |
hi all how can i connect s7 200 222cpu to winccflexible on pc ...sent from App |
tigranes |
|
5/3/2021 2:57 PM | |
Joined: 9/27/2006 Last visit: 4/25/2024 Posts: 12257 Rating: (2665) |
Hello tigranes; When you say "WinCC Flexible on PC", you mean a WinCC Flexibe RT (runtime) installation, correct? Which version of WinCC Flexible do you have, and which version of S7-Microwin are you using to program the S7-222? This document will provide good basic information on the connection options you are asking about: - What should you watch out for when setting up a connection between S7-200 and SIMATIC Panels or WinCC flexible PC Runtime and what are the options? https://support.industry.siemens.com/cs/ww/en/view/28263099 Do not hesitate to come back to the forum if you need more specific information. Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
Follow us on