5/6/2021 2:26 PM | |
Joined: 4/14/2020 Last visit: 7/10/2023 Posts: 1 Rating: (0) |
Hello guys, We have a problem with setting up ip address at pxc50-e.d. PC ip address=192.168.1.10 We use FW: V6.00.314 and we are running xWorks V6.1 on VirtualBox. In the beginning, we had the same problem and after a lot of trying and changing settings, we were somehow able to configure PLC IP address but we were unsure what we did that made the difference and now, after few days, with no settings changed, we can't configure the ip address anymore and the same problem we had in the beginning persists. We would like to set up pxc50-e.d. address to 192.168.1.80. First of all, we click "search all" and our PLC with default IP address appears as you can see on the picture. In the attachment is figure and you can see that every LED on power module, 24vdc and 24vac, is on. Also you can see two more figures, PLC with default IP address and with configuration error. Best regards! AttachmentDesktop.zip (233 Downloads) |
Last edited by: shorina at: 05/06/2021 14:39:08Last edited by: shorina at: 05/06/2021 14:40:00 |
|
5/7/2021 9:29 AM | |
Posts: 39 Rating: (8) |
You can also check the "Real PC's" IP address range. |
Follow us on