Industry Online Support
Technical Forum
3/2/2009 9:33 PM | |
Posts: 2661 Rating: (279)
|
Have you seen the following? Error message: "Cannot access desired OPC server. ... Class not registered" |
This contribution was helpful to1 thankful Users |
3/3/2009 1:30 PM | |
Posts: 54 Rating: (2) |
Dear Phantom Thanks for your reply. In actual I have done the OPC DCOM config when the runtime is not active. Now I have redone and checked the settings in WinCC runtime. As per the FAQ, the settings were made for both OPC server & OPC Enum. But still the error exist. Im attaching the screen dump of the DCOM settings. I have added the following user groups in the access limits of DCOM config: administrators, system, interactive, anonymous logon, network etc. Regards, Kanag AttachmentOPC_SET_2.zip (455 Downloads) |
3/24/2009 10:00 PM | |
Posts: 2661 Rating: (279)
|
Hi Kanag, Install WinCC + connectivity pack and do not change any DCOM settings. See if it works. Regards |
This contribution was helpful to1 thankful Users |
Follow us on