3/23/2009 6:49 PM | |
Posts: 2 Rating: (0) |
Hi all, I have a problem to connect a Cognex camera with a CPU315 2DP/PN. I configure the PLC and the camera with HWConfig, i use the last version V2.6 for the PLC and the last GSD file for the cognex camera. (you can find it in attachment). I transfert this configuration and before i put the PLC to RUN mode, the SF and BF2 leds was red. In the diagnostic of PLC, i have this event: ID event: 16#596D, adress module: 2044 (it's the adress of controler IO), error: incorrect mode for ProfinetIO, state: stop(internal). but the camera have no error. when i check the ethernet partner, the software see the camera with the good name and the good IP adress. Do you have an idea of my problem? bad GSD, no compatible version,.... Thanks for helps. AttachmentInSightGSDnESDFiles.zip (382 Downloads) |
3/24/2009 9:25 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello Assuming that everything in cognex 5000' configuration is OK, I suggest you to look at Why does the LED BF2 light with PROFINET CPUs S7-315/317-2PN/DP V2.3 even though no bus fault can be determined? Hope this will helps! regards |
Follow us on