Industry Online Support
Technical Forum
4/8/2009 3:04 PM | |
Posts: 11 Rating: (0) |
I want to communicate MM440 and CPU S7 313C, but i dont know how, someone help me. Thanks |
4/8/2009 3:20 PM | |
Joined: 9/28/2005 Last visit: 8/27/2024 Posts: 2957 Rating: (242) |
Hi, You can control MM440 drives using Profibus-DP or USS protocol. Your CPU has MPI only. So you need communication processor (CP). For Profibus-DP you need CP342-5 and for USS or Modbus you need CP-341 (or CP-340 if you write driver by yourself). If you decide to use profibus, then you can find examples of controlling Micromaster drives here: http://support.automation.siemens.com/WW/view/en/22078757 http://support.automation.siemens.com/WW/view/en/22318171 If you decide to stay with USS or Modbus then don't forget that you need to write driver by yourself (for CP-340, CP-341) or you need it to buy from siemens (for CP-341 only). |
Best regards, |
|
4/9/2009 9:44 AM | |
Posts: 11 Rating: (0) |
Okey, thanks all. I decided to use Profibus DP cause i also have to use an ET200 for distributed control. |
Follow us on