5/3/2009 8:58 AM | |
Joined: 9/27/2006 Last visit: 5/8/2024 Posts: 12257 Rating: (2666) |
Hello kumar; Siplus is an electronicboard design certification that denotes high-temperature range, medial coating (resistance to harsh environments) and high resistance to vibrations for the modules selected. As such, there are no manuals specifically for Siplus units, they behave exactly as their standard equivalents. You should provide the standard manual for each (for example the S7-300 Module Data manual will give youspecifications for all signal modules, analog and digital) plus the datasheet or Certfication sheet for each module. The following link will take you to the Siemens Siplus portal, with information on the Siplus part number and the equivalent standard part number of all Siplus units. It will also provide details on the level of protection given to the specific part numbers. https://www.automation.siemens.com/siplus/html_76/produkte/s7300.htm Hope this helps, Daniel Chartier |
Follow us on