Industry Online Support
Technical Forum
5/6/2009 9:03 AM | |
Posts: 16 Rating: (0) |
Hi, According to the following link in IA DT Service Support http://support.automation.siemens.com/WW/view/en/35362864 The free function blocks (Free Blocks) have not been released for the following SINAMICS S120 devices: - SINAMICS S120 <= 250kW The free function blocks (Free Blocks) have been released for the following SINAMICS S120 devices, Firmware Version V2.4 (or later): - SINAMICS S120 Cabinet Modules - SINAMICS S120 > 250kW How is this possible if the CU is the same CU320for all S120 systems!!!! |
5/6/2009 12:04 PM | |
Joined: 5/7/2008 Last visit: 3/29/2024 Posts: 41 Rating: (2) |
Hello! FFB are assigned to Power Modules not for CU. |
6/2/2009 5:49 AM | |
Posts: 16 Rating: (0) |
Hi, |
Follow us on