6/4/2009 9:54 AM | |
Joined: 9/28/2005 Last visit: 3/12/2024 Posts: 2957 Rating: (242) |
Hi, Its very hard to say what's the problem not having configuration of the project. It could be some problems with configuration or with password. I can only suggest to change password to something simplier like 1234, then reset existing password on OP and download project with new password and the try to see what's happening. Also look this link. Maybe it will be helpful http://support.automation.siemens.com/WW/view/en/24141925 |
Best regards, |
|
This contribution was helpful to1 thankful Users |
6/4/2009 11:05 AM | |
Joined: 9/7/2007 Last visit: 8/30/2023 Posts: 550 Rating: (61) |
Hi coopdegrace |
Best Regards |
|
Follow us on