6/16/2009 12:00 PM | |
Joined: 6/13/2006 Last visit: 2/11/2023 Posts: 341 Rating: (24) |
You can't upgrade directly to V7.0 . You would have to first upgrade to V6.2 then V7.0. See following FAQ http://support.automation.siemens.com/WW/view/en/25473507 Regards, rit03 |
6/16/2009 12:22 PM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating: (102)
|
Hi For an upgrade you should use the newest version, that means WinCC V7.0 SP1. In the attachment you find a part of the installatiion notes of the doku. You have to upgrade twice, form v5.x to v6.0 and v6.0 to v7.0. You find the migration in the doku under: First Steps > Upgrading WinCC WinCC V6.2 HMI Manual Collection: (press at "info") http://support.automation.siemens.com/WW/view/de/25842925 WinCC V6.2 SP2 / V7.0 HMI Manual Collection: (press at "info")http://support.automation.siemens.com/WW/view/en/29489481 regards cumulus |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|
Follow us on