7/6/2009 12:58 AM | |
Posts: 34 Rating: (0) |
Hello , Does Siemens have block for Sentron PAC series ? Or do we need to design on our own bye, |
7/6/2009 1:35 AM | |
Joined: 10/7/2005 Last visit: 4/18/2024 Posts: 3003 Rating: (1046) |
Kello Kucuk a block to do what? The PAC3200 is a "simple" DP Slave, so you'll get all values of interest from itvia cylic data by simple HWconfig just as with any other DP Slave. You decide which values you want to read when you configure it in HWconfig. I'd recommend to setup Basic Type 1 and/or 2 and then add any other values to it that you want to read out on top of what's included in the baisc types (there are no dat sets or data records to be read via acyclic DPV1 function, so no need tostart programming SFC58/59 or SFB52/53). Have a look at this Profibus DP expansion module manual for the PAC3200 which details itall very neatly. If you use however WinCC as the SCADA system you can additonally havelook at the (rather expensive) WinCC powerrate which will give you quite a few pre-programmed S7 Blocks and corresponding WinCC faceplates (and a few more features such as Excel report templates, I haven't used it yet though and can't make any "value added" statements, you can find the powerate manual here). I hope this helps |
Last edited by: fritz at: 7/6/2009 1:36 AMCheers |
|
This contribution was helpful to3 thankful Users |
7/6/2009 12:24 PM | |
Posts: 34 Rating: (0) |
Hello fritz, thank you for your answer, I meant to say "have it as Wincc Powerrate ," sentron is simple, so I think we need to create our own blocks regards, |
7/7/2009 3:32 PM | |
Posts: 34 Rating: (0) |
Thank you Ayman, Yes, Its easy to put on simatic hardware, Then I will configure as I need , L1-L2 then Frequency ... however I want regards |
7/12/2009 7:04 PM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (835) |
Hello again, |
Last edited by: Ayman Elotaify at: 7/12/2009 7:05 PMLast edited by: Ayman Elotaify at: 7/12/2009 7:04 PMAyman Elotaify |
|
Follow us on