Industry Online Support
Technical Forum
7/13/2009 10:02 PM | |
Posts: 89 Rating: (1) |
How to connect Field PG to the Logo PLC and how to diagnose the fault which software should be in the FPG for diagnosis. |
7/13/2009 10:14 PM | |
Joined: 3/25/2008 Last visit: 1/28/2022 Posts: 232 Rating: (19) |
Hi there. Best Regards. |
Keep working! |
|
7/14/2009 5:11 PM | |
Posts: 173 Rating: (95) |
"Diagnosis of LOGO!" Hi mohit & TEBANCH 1) on the PG or any other PC or laptop, you need the LOGO! software. This is called 'LOGO! Soft Comfort'. The current version is V6.1. To do 'diagnosis' you need a full installed licensed version, not the demo. 2) You can buy it from your LOGO! supplier. The part number is 6ED1 058-0BA02-0YA0. The latest Service Pack and different language files can be downloaded from https://www.automation.siemens.com/logo/html_76/support/01ToolsDownloads/index.html 3) Different language manuals can be downloaded directly from https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=36051989&caller=view (click the small down arrow next to 'more languages') 4) When you install the software (it is not automatically available on PG's, it must be bought and installed separately), there will be an option to install the USB cable driver - do this. 5) To connect to the LOGO!, you need either a RS232 COM port cable, part number 6ED1-057-1AA00-0BA0 or the USB PC Cable part number 6ED1 057-1AA01-0BA0. 6) The RS232 version can connect directly tothe 9 pin COM port on the PG or other PC. If there is not a 9 pin COM port, then you can use the USB PC Cable or you can use an externally supplied USB to COM converter cable. For this or the USB cable, you will have to install the driver (as mentioned above) 7) When you connect the LOGO! to the PG or PC, you can then start the software. You might need to go to the TOOLS menu option, then to OPTIONS, then to INTERFACE to either automatically select the COM port number that the LOGO! is connected on 8) Then you can communicate with the LOGO! and upload the program that is already on it, or compare the program that is on there to the originally written program if you have a backup of it from the original developer 9) then you can start with your 'diagnostics'. Otherwise you can send questions to this forum to help further! Cheers Barbarian! |
Follow us on