6/22/2009 1:30 PM | |
Joined: 5/28/2008 Last visit: 12/8/2015 Posts: 901 Rating: (136) |
Hello, in Service & Support Portal you only find the last HF or SP of the WinCC version. In this task SP3. Here the link: http://support.automation.siemens.com/WW/view/en/35958594 If you need SP2 then try to contact the Hotline from Siemens. Maybe they could help you... https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.cssr&siteid=csius&lang=de&aktprim=100&content=support/newSR/index.asp regards manfred |
6/22/2009 1:48 PM | |
Joined: 6/13/2006 Last visit: 2/11/2023 Posts: 341 Rating: (24) |
You can Order SP2 for WinCC 6.2 free of chargeat following link. All you need your WinCC 6.2 License number. |
Last edited by: rit03 at: 6/22/2009 1:49 PM |
|
This contribution was helpful to2 thankful Users |
6/22/2009 1:58 PM | |||
Joined: 4/5/2006 Last visit: 9/16/2024 Posts: 917 Rating: (63) |
Hi fazal, if you already have WinCC v6.2 you can use support link to order SP2, it 5 days maximum (or less) to receive CD/DVD and it's free
Regards |
||
6/22/2009 2:31 PM | |||||
Joined: 4/5/2006 Last visit: 9/16/2024 Posts: 917 Rating: (63) |
Hi fazal, i don't think you can download SP2 ONLY: download doesn't work like Windows update, not in this cases at least (SP2 is very big), but delivery is very fast At the end, i forgot to tell to download this HF too (patch 3 is very important)
Regards |
||||
7/20/2009 12:18 PM | |
Posts: 35 Rating: (0) |
Thank you so much every one for the support. I ordered the SP2 online and got it within 7 days ! Cheers |
Follow us on