7/28/2009 7:56 PM | |
Posts: 8946 Rating: (999) |
New Bitmap Image.jpgis not a vailf jpg. |
7/29/2009 11:02 AM | |
Joined: 10/7/2005 Last visit: 4/24/2024 Posts: 3004 Rating: (1046) |
It depends lalit I would at least check if the two outputs bits ("Global_DB".SYS_1SEC_TICK and "Global_DB"SYS_2SEC_TICK) are NOT used anyhwere else in the program, before you remove this logic. And even if they aren't,itnever "hurts" to have at least a 1 second'tick" (think using it for simple things like valve openingtimecounting andthe likes) and I'd probably rather assign MB4 as the CPU clock memory byte (instead of removing the logic). I always use the CPU clock memory byte and make all its bits available as as (oneshot) "ticks' or "spikes" or whatever you want to call them, simply beacuse it's "better to look at them than to look for them" should the need arise. |
Cheers |
|
Follow us on