Industry Online Support
Technical Forum
8/28/2009 12:58 AM | |
Joined: 10/7/2005 Last visit: 9/19/2024 Posts: 3021 Rating: (1054) |
Hello Inst_Tech Data type TIME is simply a Double Integer which holds a millisecond value, examples are: T#1s = 10000 T#1m = 60000 T#3m5s10ms =185010 As such, you simply convert your REAL to a DINT(e.g. ROUND instructions) and use te result as the TIME (and if you want to have seconds on your HMI/REAL variable, multiply it with 1000 before youROUNDit to a DINT). I hope this helps |
Cheers |
|
This contribution was helpful to3 thankful Users |
8/28/2009 6:48 AM | |
Posts: 2 Rating: (0) |
That is very helpful. I was starting to clue in to this solution. I will attempt to implement this at work. Thank you |
Follow us on