Industry Online Support
Technical Forum
8/26/2008 1:59 PM | |
Posts: 133 Rating: (2) |
hi! have you configured setting of software to connect to device via port15? |
8/26/2008 2:15 PM | |
Joined: 9/9/2007 Last visit: 8/12/2021 Posts: 27 Rating: (0) |
wich settings did you mean? |
Last edited by: MDehshat at: 8/26/2008 2:17 PM |
|
9/21/2009 8:31 AM | |
Posts: 3 Rating: (0) |
Hi I had same problem, And I could able to solve the issue. Basically USB PC adaptor will require external 24VDC. There is a cable available from siemens which will have connection for external supply. Otherwise just supply 0VDC on pin no:2 and 24VDC on pin no: 7 of the adaptor MPI/DP port side. This will power the adaptor. And then it will communicate with any device which doesnot haveoption to supply 24VDC supply. Make sure that youuse class 2 power supply.otherwise this may damage the adaptor. Otherwise To usestandard cable from siemens, To operate the PC Adapter USB to MPI/DP interfaces which do not have a 24V supply voltage, you can order an external power supply (order number: 6ES7 972-0CA00-0XA0). AttachmentPC_Adapter_USB_e.pdf (700 Downloads) |
Follow us on