Industry Online Support
Technical Forum
9/28/2009 4:17 AM | |
Joined: 6/20/2008 Last visit: 2/19/2024 Posts: 73 Rating: (1) |
Hi All, I am facing problem with Client project in WinCC V6.2SP2 on WinXP SP2: - My system has 2 project: WinCC Server project running on Server and WinCC Client Project running on Client - Server is istalled withWindows server 2k3 SP2, Client is installed with Windows SP SP2 - When Client project is running, the graphic screen is out of desktop. Then i open my client project, the project is still activated(see Pics 1 as below). I also check the status of Server connections , it said that the Connection Status is established(see Pics 2 as below). I have opened a graphic which is Start Picture of WinCC and runtime this graphic then the graphic screen is on OK on desktop of Client. But it is a cycle about 2 days the grapic screen is out of desktop again. I don't know how to resolve this problem. I am looking from all of you soon NTV AttachmentPics.zip (52 Downloads) |
9/28/2009 1:11 PM | |
Joined: 10/9/2007 Last visit: 9/18/2024 Posts: 1249 Rating: (115) |
Hi I see you are using Sicam PAS CC. Take a look at this post. On the last post there is a hotfix. I'm not sure ifit will solve your problem, so make a backup and try it. Check your version of PAS CC before using it. /tf/WW/en/Posts/31553 Mike J |
Energy Automation products: Sicam, Siprotec, Digsi |
|
Follow us on