Industry Online Support
Technical Forum
3/26/2008 12:00 PM | |
Posts: 4 Rating: (0) |
Hi, I have a MP277 touch 10''. I need to archive data in a shared folder on a PC Server. The panel is conected to an ethernet network. I think that the network configuration on MP277 is correct (IP address, subnet mask, gateway and DNS) becausein the command prompt on MP277 with the command "ping" I get reply from the PC Server, I useping commandwith thePC names.(you can see this on ping.jpg). In thePC Sever I've created a share folder withname "prueba" andI give all permiss to the same user that I configure on the Network ID on the MP277. From another PC and using this user, I connect to the share folder on the PC Serverwhithout problems. But if I try to connect to PC Sever from MP277 I get the message that path is incorrect. (you can see this on error.jpg). If the runtime starts in the diagnostics buffer I get theerror number 80015 "the system cannot find the drive especified". I think that the problem is on Network ID on the MP277. When I configure it, I fill in the user name, the password and the domain, but when I come back and open it again the password is null. (you can see this on networkID.jpg). Is this normal? Do you have any idea? Thank you for your help and I am sorry for my english. Attachmentimages.zip (86 Downloads) |
3/27/2008 1:38 PM | |
Joined: 5/8/2006 Last visit: 4/19/2024 Posts: 1085 Rating: (77) |
Hi, maybe this FAQ will help you: http://support.automation.siemens.com/WW/view/de/13336639 Bye |
This contribution was helpful to1 thankful Users |
10/6/2009 5:55 AM | |
Posts: 10 Rating: (2) |
\I have posted a request for much the same problem - did this one get resolved ? /tf/WW/en/Posts/35651#top171104 Alan |
Follow us on