10/9/2009 10:35 PM | |
Posts: 3 Rating: (0) |
If you go to Entry ID 23378039 in the notes it says that this function is also available in the Profinet -IO IM's. The manual is out of date as it only deals with profibus IM's. The problem is that the hardware manager has no devices that install 12in/6out option ( Profibus or Profinet). This means that we would probably need an additional gsd. outside the standerd ones provided or something else.... I am using the IM as a cpu so it is not a remote I/O. |
Last edited by: O_Moderator at: 10/10/2009 7:26 AMlink edited |
|
Follow us on