10/23/2009 11:05 AM | |
Posts: 9 Rating: (0) |
seems like i need to update my firmware? offline v1.0 and online v2.6.9? might this cause a problem? |
10/23/2009 11:23 AM | |
Posts: 382 Rating: (47) |
Dear dezuna, Are you referring to CPU firmware? You can go online update. See attach Hope this helps! with regards, how come? |
10/26/2009 9:36 AM | |
Posts: 382 Rating: (47) |
Dear dezuna, Please look at the attach, is this the configuration you are looking for? If it is, download the program. Then open OB1 and goto online monitoring. Short your first input from the DI card to activate the first DI channel. In this example is I124.0. See whether the output Q124.0 activated? Hope this helps! with regards, how come? AttachmentTo dezuna.zip (312 Downloads) |
10/27/2009 9:11 AM | |
Posts: 382 Rating: (47) |
Hi, Glad to hear that. I hope you have solved your problem after discovering the missing wires. with regards, how come? |
Follow us on