6/3/2009 10:43 AM | |
Posts: 2 Rating: (0) |
My Logo is curently monitoring and controlling my solar hot waterboiler, i can collect actual data temperature and running hours via the online test in the Logo soft software. I would like to present the data on my computer in Visual Basic. In the future i also want to incorporate the logo in home domotica. Does anybody know how to connect to the Logo and retrive the data so i can use the data in Visual Basic. Or what is the language Siemens uses fore the communication between Logo and Logosoft. As an example i uploaded the grafics i want to use for the presentation on my computer. AttachmentIMG.pdf (1024 Downloads) |
6/3/2009 5:20 PM | |
Posts: 191 Rating: (58) |
Hi!! there is a way to save al logo variables in excel... this is the last thread i saw with this question... /tf/WW/en/Posts/30147#top maybe from excel you can use the data for visual basic... ROSA |
6/3/2009 6:05 PM | |
Posts: 2 Rating: (0) |
looks promissing wil take a look, also on the german site |
6/3/2009 8:08 PM | |
Joined: 1/5/2007 Last visit: 4/7/2023 Posts: 1690 Rating: (580)
|
Hi, here is tge directlink to the Excel Logo Logger; attachment(vrom my answer at 14.12.2008): FORUM_LogoLogger2_Test_3.zip This logger can log I/O-status and all digital flag blocks every second or slower. I am working at the second version, this can log actual block values too and comes with some additional options... Best regards Betel AttachmentFORUM_LogoLogger2_Test_3.zip (776 Downloads) |
==> Meine TAG-Listen: "deut." |
|
This contribution was helpful to1 thankful Users |
6/17/2009 6:47 PM | |
Joined: 7/15/2008 Last visit: 1/10/2024 Posts: 14 Rating: (5) |
In this link you can download the version Demo of the driver. Limitations of the version Demo: - Only supported 0BA5. - Save file no permitted. If you wish this product. Please send me the answer so I will give you the link for purchase.AttachmentDemo LOGO!view.zip (737 Downloads) |
Carlos Calderón Córdova |
|
10/30/2009 3:38 PM | |
Posts: 1 Rating: (0) |
Does it logo logger work with USB cable ??? |
Follow us on