8/29/2009 9:09 AM | |
Posts: 163 Rating: (0) |
May be my question is silly but i guess it would be of great help at this time if you clear me this concept. Attachmentconnecction types.zip (150 Downloads) |
Last edited by: Sindhu at: 8/29/2009 9:31 AM |
|
8/31/2009 2:22 PM | |
Posts: 5822 Rating: (411)
|
Dear Sindhu, actually I personally doubt that this list is right in this point. Let me think... If I configure a fault tolerant S7 Connection from my PC and I use an OPC Server on top of it I open the OPC Scout. If I check the DBs there I see them, I can getfrom or put to itany data I want. So why should GET and PUT not work here? We still have the SAPI S7 interface just a certain part of connection handling below it. Personally I doubt this statement in the list, may you tell us where you got this from? About your issue with the MP377 I guess that you have used the known function to establish your Ethernet Link from one Panel to the H-System (starting with flexible 2008 I guess)by the use of 2 Ethernet Connections. Well, I see no reason why it should not work to have 4 connections to two H-Systems instead of 2 connections to one H-System. If you are connected to the second H-System, as it is at the same Network as far as I understood, you should not have any problem to read the I/O valuse as you need it. I hope this will help you. Best regards J_Bell |
9/11/2009 7:38 AM | |
Posts: 163 Rating: (0) |
Pls find attached my program which shows errors. AttachmentP-CS-0_7.zip (123 Downloads) |
Last edited by: Sindhu at: 9/11/2009 7:49 AM |
|
Follow us on