11/18/2009 11:56 PM | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Joined: 4/19/2008 Last visit: 2/9/2024 Posts: 1525 Rating: (159) |
Hi tomy Master, Can you please Download the Step 7 V5.4 SP5 patch which is available on Siemens, Please find the link for the http://support.automation.siemens.com/WW/view/en/36184684 Please see the Compatibility list For Step 7. http://support.automation.siemens.com/WW/view/en/8250891 or Configuration notes: The following table shows you as of which version of STEP 7 there is compatibility with which Microsoft Windows operating system:
2) As from STEP 7 V5.1 incl. SP2 you require SP1 for MS Windows 2000. 3) No support planned from MS Windows XP Home. 4) MS Windows 95b or MS Windows 95 OSR2 required for OEM versions. 5) MS Windows 98 SE (Second Edition) required. 6) SP6a for MS Windows NT 4.0 required. 7) At least SP1 for MS Windows 2000 required. 8) MS Windows 2000 Professional at least SP3 required. 9) MS Windows XP Professional SP1 recommended. Not released for MS Windows XP Professional SP2. 10) MS Windows XP Professional SP1 or SP1a required. For MS Windows XP Professional SP2 you require STEP 7 V5.3 SP2. Not released under MS Windows XP SP2c. 11) STEP 7 V5.3 incl. SP2 is not enabled for use in MS Windows Server 2003 incl. SP1. 12) MS Windows Server 2003 as workstation computer, STEP 7 V5.3 SP2 required 13) MS Windows 2000 Professional SP4 required. Not released for STEP 7 V5.4 SP4. 14) MS Windows Server 2003 standard edition and MS Windows Server 2003 SP1 standard edition as workstation computer. For STEP 7 V5.4 SP4 Windows Server 2003 SP2 is required. 15) MS Windows XP Professional SP1 (or SP1a) or SP2 required. For MS Windows XP Professional SP3 you require STEP 7 V5.4 SP4. Not released under MS Windows XP SP2c. 16) As of STEP 7 V5.4 SP3. STEP 7 is not released under MS Windows Vista Home Basic or Premium. Right now I have insatlled V5.4 SP4 on my laptop which is having XP SP3, please try to get the V5.4 SP4 or SP5 which will installed on XP SP3. |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Ammy |
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
This contribution was helpful to1 thankful Users |
Follow us on