Industry Online Support
Technical Forum
12/9/2009 8:17 PM | |
Posts: 38 Rating: (0) |
Hi, I am having a problem configuring the HMI on a client/server project. I am using WinCC V5.1. The server is running fine, and for the most part the client is running fine. The only problem is the circuit breaker status on the client. As shown in pic1, the client is running. It is clear that the circuit breaker status is incorrect, because it is shown as a red X. I believe the problem is the control graphic is not linked to a tag. So I go into the graphic editor and double click on the control box. I then go to the tag connections as shown in pic2. There are no tag connections for the control box so it defaults to a red X. So I go and browse for the correct tag and apply and hit ok. However, I get an authorization error as shown in pic3. Does anyone know how to change the authorization to allow the tag to stay connected? Or has anyone experienced a problem like this before? Thanks AttachmentClient Errors.zip (50 Downloads) |
Follow us on