2/11/2009 8:53 AM | |
Joined: 4/24/2006 Last visit: 9/25/2024 Posts: 8742 Rating: (1168) |
Dear Roby, Here is a solution for panels which can use scripting: http://support.automation.siemens.com/WW/view/en/24141925 Here are some tips and tricks: http://support.automation.siemens.com/WW/view/en/24455368 Make sure you have another Administrator, so you can put the users which are unauthorised, again in the authorised group. When you use WinCC flexible 2008, you can change the number of wrong inputs. See link: http://support.automation.siemens.com/WW/view/en/29735640 Point 2 Best regards, Wizard |
2/11/2009 2:18 PM | |
Joined: 4/24/2006 Last visit: 9/25/2024 Posts: 8742 Rating: (1168) |
Hi Roby, The standard password is 100 and username Admin. Best regards, Wizard |
Follow us on