Industry Online Support
Technical Forum
7/21/2009 11:57 AM | |
Posts: 157 Rating: (10) |
Dear experts, I want to implement a SCADA system with the following topology: 1- One WinCC server. 2- One Archive Server. 3- Two clients. I have WinCC v7.0 SP1... The problem which faced me is the "Archive Server". To solve this problem i read about WinCC/CAS (Central Archive Server) option. But i can't find an easy and integrated description about WinCC/CAS, and how to do it and link it with The WinCC server and the clients. I found one, unfortunately it was in Russian language.. http://www.automation-drives.ru/as/download/ascat/simatic_hmi/wincc/WinCC_CAS_ru.pdf Please any help please.. Or if any one can translate this document to English.. Another thing... If i have a project and i want to view the archive data from another project linked together with ETHERNET network.. what should i do?? Thanks, Yours, Bilal Dweik |
7/25/2009 2:33 PM | |
Posts: 157 Rating: (10) |
Any Help Please . . . . |
8/9/2009 12:30 PM | |
Posts: 157 Rating: (10) |
Are You There Experts???? |
8/18/2009 11:16 AM | |
Posts: 157 Rating: (10) |
Dear marcell, I hope one of the experts here help us in this problem... Regard, BilalD |
2/6/2010 1:32 PM | |
Posts: 157 Rating: (10) |
To help others.. and here you can download the Wincc/CAS 7.0 SP1 Regards, |
Last edited by: BilalD at: 2/6/2010 1:36 PM |
|
Follow us on